cancel
Showing results for 
Search instead for 
Did you mean: 

Migrating from STVD7 3.1.1 to 3.3.2

stock_vaber
Associate
Posted on July 10, 2006 at 14:02

Migrating from STVD7 3.1.1 to 3.3.2

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
stock_vaber
Associate
Posted on June 19, 2006 at 15:05

I have just downloaded the last release 3.3.2 of STVD7.

A workspace saved with STVD7 3.1.1 is no more compilable (I have Cosmic 16K-limited free compiler).

It seems that the compiler is launched with a wrong command string: the path of the compiler include folder does not have the '-i' prefix, so the compiler takes the path as a wrong file name and exits with an error.

Instead, the tutorial examples are compiled well, the compiler include folder path has the '-i' prefix, so I think is an import matter of the project file .stp.

Do you know the right procedure to import 3.1.1 workspaces in STVD7 3.3.2?

sjo
Associate II
Posted on June 20, 2006 at 11:42

If i get problems with upgrading to a newer version of Visual Develop i find pressing the defaults button on the various project settings tabs fixes the problem.

Regards

sjo

emmanuel23
Associate II
Posted on July 10, 2006 at 14:02

Hi,

When we meet such problems during integration phase, we often see that opening the project settings, navigating in each tab, and clicking on OK is enough to fix the issue.

Anyway, this should not happen.

Could you send me the *.stp.bak file (backup of the initial stp file).

So we could investigate.

Emmanuel.