cancel
Showing results for 
Search instead for 
Did you mean: 

lite_timer_interrupt&STVD7&Cosmic

irmakci2
Associate II
Posted on May 23, 2006 at 11:51

lite_timer_interrupt&STVD7&Cosmic

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
irmakci2
Associate II
Posted on May 23, 2006 at 11:51

Hi.I want to learn something about stflite0 litetimer interrupt...

I am using Cosmic C in ST7VD toolset.I need the time for scaning Display and other time dependent routines.I am using wfi()

assemblier instruction set in Cosmic C.

I want to use the program in the LiteTimer interrupt routine after some time...

I can only success in entering interrupt routine when I used the wfi()

instruction.But I couldn't success in entering without wfi() instruction...

I couldnt see entering interrupt in ST7VD toolset...But

Which vas false?

1-Can we enter litetimer interrupt routine after some time without wfi()...Because I can only see in ST7VD entering with wfi() but not without wfi()

Doesn't ST7VD show me entering without wfi() or Can not I see?

2-Or ,Cosmic can't handle this problem?

3-Or I have an error

Please help me

Thanks in advance