cancel
Showing results for 
Search instead for 
Did you mean: 

Is the LM311DT rail-to-rail?

AndrewIC
Associate

As per subject, is the ST LM311DT rail-to-rail? Farnell claims that it is, but that's the only place that says it is, I can't find a definitive statement in the datasheet.

(I have used the TI LM311, and that is not rail-to-rail. I need to handle inputs close to Vcc.)

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @AndrewIC, to the community!

What catalogue distributors write on their websites is their responsibility, not that of the manufacturer. The respective data sheet is always decisive for technical parameters. But even rail-to-rail is not a clear specification, because it does not say whether it refers to the input or the output.

In this case, it is a voltage comparator that was developed in the last millennium and still uses bipolar technology. If you look at the electrical characteristics in table 4 of the data sheet, you will find the input common mode voltage range, which is specified as VCC=±15V with a typical value of -14.7...+13.8V, and +13V in the worst case. It is precisely this difference, which can be up to 2V, that indicates that there is no RR-I.

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @AndrewIC, to the community!

What catalogue distributors write on their websites is their responsibility, not that of the manufacturer. The respective data sheet is always decisive for technical parameters. But even rail-to-rail is not a clear specification, because it does not say whether it refers to the input or the output.

In this case, it is a voltage comparator that was developed in the last millennium and still uses bipolar technology. If you look at the electrical characteristics in table 4 of the data sheet, you will find the input common mode voltage range, which is specified as VCC=±15V with a typical value of -14.7...+13.8V, and +13V in the worst case. It is precisely this difference, which can be up to 2V, that indicates that there is no RR-I.

Regards
/Peter

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you Peter, that's exactly what I needed. The was the common mode range is expressed in the ST data sheet wasn't clear to me - I have seen other manufacturers' data sheets specify the upper limit of the common mode voltage as e.g. "Vcc+ minus 2.0V", but what you have said makes perfect sense.

Regards
Andrew