cancel
Showing results for 
Search instead for 
Did you mean: 

Is STW13NK100Z available as an SMD?

GBobe.1
Associate

trying to avoid through hole part, would prefer a SMD part.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @GBobe.1​, to the community!

This STW13NK100Z with exactly the same parameters is not available as SMD, but you can look at the STH12N120K5-2, which has a slightly higher Rdson, but can even switch 1200V instead of only 1000V.

The only other alternative in this voltage class would be the same device STH13N120K5-2AG with essentially the same parameters, but with automotive approval.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @GBobe.1​, to the community!

This STW13NK100Z with exactly the same parameters is not available as SMD, but you can look at the STH12N120K5-2, which has a slightly higher Rdson, but can even switch 1200V instead of only 1000V.

The only other alternative in this voltage class would be the same device STH13N120K5-2AG with essentially the same parameters, but with automotive approval.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.