cancel
Showing results for 
Search instead for 
Did you mean: 

implementing a simple half duplex rs232 emulation

dhutchison1945
Associate II
Posted on June 15, 2010 at 11:27

Dear forum members,

I need to implement on a st7 mcu a simple and very slow half duplex rs232 like protocol(software emulated).

I have only the following resources available:

1 16bit timer.

1 output pin for the tx (a general purpose pin without output compare)

1 input pin for the rx(a general purpose pin without input capture but with external interrupt)

My question is: Is it possible to use the external interrupt functionality instead of the input capture

functionality for the reception ?

b.r.

Spectre

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0