cancel
Showing results for 
Search instead for 
Did you mean: 

IAP

saravan
Associate II
Posted on May 18, 2005 at 08:13

IAP

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
saravan
Associate II
Posted on May 11, 2005 at 07:07

Hi,

I am using a ST72521 MCU in my project.

I have a problem with IAP.

When i try to erase sectors it is successful.

Byte write is also succesful.

But Block Write is failing.

What are the different reasons for this problem.

Thanks,

Sarav

venkateswara
Associate II
Posted on May 18, 2005 at 08:13

you have to ensure that the parameters are passed correctly i.e. the source buffer address (located in the RAM) and the number of bytes etc. You can read the error status(returned at 0xFF) and find the exact error. The information about the error status is given in the ST7 flash programming manual. You can also try with a higher FREQ value.

regards,

venky