2009-03-02 11:09 PM
I2C lines
2011-05-17 6:02 AM
Hi
what differents are there bitween open drain and true open drain outputs ? should SDA and SCL i2c pins to be true open drain type or not require if they want to work right application? thanks and regards2011-05-17 6:02 AM
Hi,
the I/O configuration true open drain output is used by default on the I/O that need alternate function output. An alternate function output can be push-pull or pseudo-open drain depending on the peripheral and Control register 1 (Px_CR1) and slope can be controlled depending on the Control register 2 (Px_CR2) values. The alternate function output(true open drain output) configuration is not accessible by configure the controle register to the user, but is by default on the IP I/O that need this configuration when is enabled. So, The SDA pin on I2C is by default true open drain output and you don't need to configure it. Regards mozra2011-05-17 6:02 AM
Hi,
I tried to use PC.5/PC.6 as SCL/SDA pins of bit-banging I2C instead of STM8S103F3 built-in hardware I2C mechanism.void GPIO_Init (void)
{ // Init Port A GPIOA->DDR = 0x08; // Set pin PA.3 output mode GPIOA->CR1 = 0x08; // Set pin PA.3 pull-up GPIOA->CR2 = 0x08; // Set pin PA.3 fast slope(max 10Mhz)// Init Port C
/* [2]101 7 6 5 4 3 2 1 0 | | | | | | | | | | | | |_______ VR0 (Output) Push pull output | | |___________ I2C SCL (Output) Open drain output | |_____________ I2C SDA (Output) Open drain output |_______________ VS (Input) Pull-up with interrupt DDR 0 1 1 0 1 0 0 0 CR1 1 0 0 0 1 0 0 0 CR2 1 0 0 0 0 0 0 0 */ GPIOC->DDR = 0x68; GPIOC->CR1 = 0x88; GPIOC->CR2 = 0x80;// Setup Port D
/* [2]101 7 6 5 4 3 2 1 0 | | | | | | | | | | | |_________ VR0 (Output) Push pull output | | |___________ VR1 (Output) Push pull output | |_____________ VR2 (Output) Push pull output DDR 0 1 1 0 0 0 0 0 CR1 0 1 1 0 0 0 0 0 CR2 0 0 0 0 0 0 0 0 */ GPIOD->DDR = 0x70; GPIOD->CR1 = 0x70; GPIOD->CR2 = 0x00; }bool I2C_GetSDA (void)
{ u8 bSDA;// Init Port C
/* [2]101 7 6 5 4 3 2 1 0 | | | | | | | | | | | | |_______ VR0 (Output) Push pull output | | |___________ I2C SCL (Output) Push pull output | |_____________ I2C SDA (Input) Floating without interrupt |_______________ VS (Input) Pull-up with interrupt DDR 0 0 1 0 1 0 0 0 CR1 1 0 1 0 1 0 0 0 CR2 1 0 0 0 0 0 0 0 */ //GPIOC->DDR = 0x28; // Case(1)bSDA = GPIOC->IDR & 0x40;
// Init Port C
/* [2]101 7 6 5 4 3 2 1 0 | | | | | | | | | | | | |_______ VR0 (Output) Push pull output | | |___________ I2C SCL (Output) Open drain output | |_____________ I2C SDA (Output) Open drain output |_______________ VS (Input) Pull-up with interrupt DDR 0 1 1 0 1 0 0 0 CR1 1 0 0 0 1 0 0 0 CR2 1 0 0 0 0 0 0 0 */ //GPIOC->DDR = 0x68; // Case(2)return( bSDA );
} /* I2C_GetSDA */Do you mean that the Case(1) and Case(2) can be
removed ? Is it possible to use STM8S103F3 PB.4/PB.5 as bit-banging I2C SCL/SDA ? Q1) How to implement bit-banging I2C using STM8S103F3 ? Q2) Can the STM8S103F3 support the quasi-bidirection pins as 8051 MCU ? Q3) Can PB4/PB.5 be used as PC.5/PC.6 for bit-banging I2C pins ? Q4) May I use PB4/PB.5 be used as normal open drain pins instead of I2C ? How to setup it ?2011-05-17 6:02 AM
Hi,
We used the SDA to read/write I2C data. Do we need to re-configure the DDR direction for Input/Output data ?2011-05-17 6:02 AM
Hi,
The I2C pins is by default true open drain output and you don't need to configure it. This configuration is forced internally when enabling the peripheral and the values in the DDR, CR... registers are not significant (by default you see that the I/O is configured as floating input) Regards mozraWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.