2005-07-26 1:54 PM
2005-07-04 6:01 PM
Default the BIOS startup at a splashscreen , it hide the start information such as memory test,PCI device table. I can close
splash screen in BIOS setup, But It is not convenience. How can I make the default bios config like AMI's config tool?2005-07-04 8:41 PM
Are you using an evaluation board? If yes, you should have a jumper to clear the CMOS.
You have also the possibility to reset the setting from the splashscreen in the bios setup.2005-07-09 5:31 AM
Yes, I use the evlboard. I clear the BIOS setup and resetup it. , such as disable spalsh, change Boot disk.....
But ofter few days , when I open the power, the BIOS has changed to default setup. I check the battary, the voltage is OK.3.2V. Why? Perhaps the BIOS is a evalBIOS, so it has some limited?2005-07-26 1:54 PM
If I recall correctly, there is a BIOS menu item that documents what are the different features in the demo BIOS from the regular one. Some timed features.
On the 4.3 version of the BIOS I remember that the board was going in halt mode after a while, with a message sayind ''demo timeout'', preventing the installation of any large operating system.