cancel
Showing results for 
Search instead for 
Did you mean: 

High optimization of IAR Embedded Workbench 9.60.3

Abdul_Aziz
Associate

What does the 'High' optimization  actually do in IAR Embedded Workbench 9.60.3 when the 'Size' option is selected, but no additional optimization checkboxes are enabled. Even without selecting any extra options(like CSE, loop unrolling, etc. ), the code size reduces significantly—up to 30%. How is the  IAR Embedded Workbench 9.60.3 achieving this reduction, and what specific optimizations are being performed in this case.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Abdul_Aziz, to the community!

the IAR Embedded Workbench is a product of IAR, so this question can probably only be answered by someone from IAR, if they happen to be reading here.

But it would probably be better if you asked the support of IAR?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Abdul_Aziz, to the community!

the IAR Embedded Workbench is a product of IAR, so this question can probably only be answered by someone from IAR, if they happen to be reading here.

But it would probably be better if you asked the support of IAR?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.