cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I need TJ(Junction Temperature) and RJA( Junction to ambient Thermal resistance) of M24C02-RMN6TP EEPROM for Derating. Can you provide. Regards, Srinivas

SJ.8
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

This EEPROM has a maximum current consumption of 1mA at 5.5V. We are therefore talking about a maximum power loss of 1mA*5.5V=5.5mW.

Even if we assume a completely unrealistic value of 100K/W for Rja, this would result in a temperature increase of 0.55K. In this respect, the ambient temperature can be regarded as identical to the junction temperature. Calculating a derating on this basis is therefore meaningless.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.