cancel
Showing results for 
Search instead for 
Did you mean: 

header file for ST72F324

egesuita
Associate II
Posted on July 05, 2005 at 06:07

header file for ST72F324

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
egesuita
Associate II
Posted on June 13, 2005 at 20:18

Hi everybody,

MCU type ST72F324 is newer respect to my ''old'' release of Cosmic C compiler so I do not have the appropriate header file for building my project.

instead of writing the header file by myself, with the risk of making some ''typos'', does anyone can send me a copy of the right one for such MCU?

Thank you very much for you precious Help

Regards

Enzo

emmanuel23
Associate II
Posted on July 05, 2005 at 06:07

You can find include files that describe peripheral registers for almost all ST7 chips in stvd7 v3.2 package (since version 3.0 in fact).

They are installed by the ST7 Toolset installation package in two different directories which are typically:

C:\Program Files\STMicroelectronics\st7toolset\include

for C header files

and

C:\Program Files\STMicroelectronics\st7toolset\asm\include

for asm files