cancel
Showing results for 
Search instead for 
Did you mean: 

EVLSTGAP3SXS-H circuit question

gammmmmm
Associate II

Hi,
Im analyzing the circuit of the STGAP3SXS in EVLSTGAP3SXS-.
I want to ask what's the purpose of this capacitance in the soft off pin, I thought it was filtering by why does it go to the VL instead of GND_ISO
Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

It may be confusing, but C14 at the pin SOFTOFF is in fact a filter capacitor. However, in terms of AC, it is also connected to GNDISO_H via C9/C10, which are more than 30,000 times larger than C14, so that it performs its filter function in exactly the same way.

However, the DC reference point for the SOFTOFF output is VL, as can be clearly seen in section 6.5 of the data sheet, for example.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

It may be confusing, but C14 at the pin SOFTOFF is in fact a filter capacitor. However, in terms of AC, it is also connected to GNDISO_H via C9/C10, which are more than 30,000 times larger than C14, so that it performs its filter function in exactly the same way.

However, the DC reference point for the SOFTOFF output is VL, as can be clearly seen in section 6.5 of the data sheet, for example.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.