cancel
Showing results for 
Search instead for 
Did you mean: 

Error L6224E while compiling AN1774 under RVDK 2.1

ewitt
Associate II
Posted on July 05, 2006 at 10:38

Error L6224E while compiling AN1774 under RVDK 2.1

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ewitt
Associate II
Posted on July 05, 2006 at 09:11

Hi,

i am trying to run the example2 code of AN1774. I am using RVDK 2.1 with RVDebug 1.7(build 380). When I open the example2.prj RVDebug converts it from a RVDK 2.0 to a RVDK 2.1 project. Now when i try to compile the project i get following Error:

Error: L6224E: Could not place 71x_lib.o(.data) in any Execution region.

I have got no clue what this means...

Some advice would be fine!

regards,

Erwin

Complete Build Output:

make -f Example2_Debug.mk all

c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armcc -c retarget.c

-g --dwarf2 -o Debug\retarget.o

License is dongled to RVI-ME

''retarget.c'', line 88: Warning: C2874W: may be used before being set

''retarget.c'', line 88: Warning: C2874W: may be used before being set

retarget.c: 2 warnings, 0 errors

c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armcc -c main.c -g --dwarf2

-o Debug\main.o

License is dongled to RVI-ME

c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armcc -c 71x_it.c

-g --dwarf2 -o Debug\71x_it.o

License is dongled to RVI-ME

c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armcc -c 71x_lib.c

-g --dwarf2 -o Debug\71x_lib.o

License is dongled to RVI-ME

c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armasm -g --dwarf2 -o

Debug\71x_vect.o 71x_vect.s

License is dongled to RVI-ME

c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armasm -g --dwarf2 -o

Debug\71x_init.o 71x_init.s

License is dongled to RVI-ME

c:\progra~1\arm\rvct\programs\2.1\526\st\win_32~1\armlink --entry Reset_Handler --scatter scat.scf Debug\retarget.o Debug\main.o Debug\71x_it.o Debug\71x_lib.o Debug\71x_vect.o Debug\71x_init.o -o Debug\Example2.axf

License is dongled to RVI-ME

Error: L6224E: Could not place 71x_lib.o(.data) in any Execution region.

Finished: 0 information, 0 warning and 1 error messages.

make: Error code 129, while making 'Debug\Example2.axf'

*** Command exited with error or warning: 255