2026-02-20 6:32 AM
Hi,
In our schematic, the IC’s SD card pin is connected to the controller pin of the STM32H753VIH6, and the IC’s controller pin is connected to the SD card. Could this connection cause any issues during SD card read and write operations? I have attached the schematic for your reference.
https://drive.google.com/drive/folders/1fHC0aW8OWq_DrnzWL8WemED_ALq8BC_0?usp=sharing
2026-02-20 6:46 AM
It looks to be symmetric to me. All of those data lines are bi-directional. Should work fine.
2026-02-23 12:39 AM
Hi,
Normal connections of EMIF06-HMC02F2 is:
If I well understood your schematic, it is connected like that, so it's good.
One question: are pull-up resistors inside STM32H753ViH6 disabled (as they are on EMIF06-HMC02F2)?
Best regards.
Fabrice.