cancel
Showing results for 
Search instead for 
Did you mean: 

EMI access in STR9

dotdotdog
Associate II
Posted on December 16, 2008 at 14:27

EMI access in STR9

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
dotdotdog
Associate II
Posted on December 16, 2008 at 14:27

I need to address the ext. memory (21e00000) in ST91x. I have configured the EMI as follow but still failed~ can you help me?

GPIO_InitTypeDef GPIO_InitStructure;

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 |GPIO_Pin_6 | GPIO_Pin_7;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt3;

GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable;

GPIO_Init (GPIO5, &GPIO_InitStructure);

GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_All;

GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2;

GPIO_InitStructure.GPIO_IPInputConnected = GPIO_IPInputConnected_Disable;

GPIO_Init (GPIO7, &GPIO_InitStructure);

GPIO_Init (GPIO8, &GPIO_InitStructure);

GPIO_Init (GPIO9, &GPIO_InitStructure);

// those bastards. this one pin out of 24 is on a different alt bus

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7;

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt3;

GPIO_Init (GPIO7, &GPIO_InitStructure);

// configure SCU

SCU_EMIModeConfig(SCU_EMI_DEMUX);

SCU_EMIBCLKDivisorConfig(SCU_EMIBCLK_Div1); // or SCU_EMIBCLK_Div1;

SCU->GPIOEMI = 1; // enable ports 8 & 9 for EMI

GPIO_EMIConfig( ENABLE );

/* Enable EMI clock */

EMI_DeInit();

EMI_StructInit( &eMI_InitStruct );

eMI_InitStruct.EMI_Bank_MemWidth = EMI_Width_HalfWord;

eMI_InitStruct.EMI_Bank_IDCY =0x6;

eMI_InitStruct.EMI_Bank_WSTRD =0x6;

eMI_InitStruct.EMI_Bank_WSTWR =0x6;

eMI_InitStruct.EMI_Bank_WSTROEN=0x6;

eMI_InitStruct.EMI_Bank_WSTWEN=0x08;

eMI_InitStruct.EMI_Bank_MemWidth=EMI_Width_HalfWord;

EMI_Init( EMI_Bank1, &eMI_InitStruct );