cancel
Showing results for 
Search instead for 
Did you mean: 

Eeprom M93C86-WMN6 with µC TI TMS320F28069 R/W does not work reliably.

GBork.1
Associate

Hello team,

I refer to a former posting from

  MVoge, June 4, 2019 at 10:16 AM

As far as I can see from that thread, the timing question have bee cleared.

Nevertheless, our problem persists (I'm continuing Marcel's work).

This is, reading back values after writing often results in readings

like 0xFFFF, 0xC7FF or 0x1FFF (most bits set!). From this, I conclude (or presume) that

writing goes wrong rather than reading.

All I can do now is sending the code of our R/W routines - I can't find anything

wrong in that code - perhaps you can... Please note that

the granularity of eeprom AND our µC is 16 bit. Please find the code attached here.

The attached file contains the implementation of the eeprom operating commands.

BR

Goetz

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0