cancel
Showing results for 
Search instead for 
Did you mean: 

Diode Zener

Jamer
Associate II

Hi,

 

Im trying to track down a couple of diodes to repair a card.  The markings are  EV Z551

 

It also has the ST logo on it, surface mount..  Anyone know where I can obtain some..

 

Cheers

 

Kev

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Jamer, to the community!

Unfortunately, you have not included a legible photo, but if the marking EV is indeed on the device, it is the SM6T36A. By the way: it is not a Zener, but a TVS = Transient Voltage Suppressor.

If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Peter BENSCH
ST Employee

Welcome @Jamer, to the community!

Unfortunately, you have not included a legible photo, but if the marking EV is indeed on the device, it is the SM6T36A. By the way: it is not a Zener, but a TVS = Transient Voltage Suppressor.

If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Peter,

 

Thanks for quick reply...

Its defo two pole device. surface mount.

 

Will Attach photo

Peter BENSCH
ST Employee

Ok, blurred and not very legible, but the package is already the right one. Yes, it is probably the SM6T36A mentioned before.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jamer
Associate II

Any idea best place to get one, RS dont have, but maybe FEC

Jamer
Associate II

Got it....

 

FEC

 

Many thanks for your help

Great!
If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.