cancel
Showing results for 
Search instead for 
Did you mean: 

Can the LM258A operate from a split supply? I'm looking at an application that would require a -5V and +16V split supply.

PC1
Associate II
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Yes, of course. It can work in the whole range of 3...30V, which is the possible voltage difference between VCC+ and VCC-. It doesn't matter, if it is

  • VCC+=0V and VCC-=30V (i.e. working below zero volts) or
  • VCC+=30V and VCC-=0V (i.e. working above zero volts) or
  • anything between, with the max difference of 30V (absolute max 32V)

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Yes, of course. It can work in the whole range of 3...30V, which is the possible voltage difference between VCC+ and VCC-. It doesn't matter, if it is

  • VCC+=0V and VCC-=30V (i.e. working below zero volts) or
  • VCC+=30V and VCC-=0V (i.e. working above zero volts) or
  • anything between, with the max difference of 30V (absolute max 32V)

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Yes. I thought that was the case, but wanted to confirm. Thank you.