cancel
Showing results for 
Search instead for 
Did you mean: 

boot and main flash?

hpaskal
Associate II
Posted on June 21, 2004 at 09:24

boot and main flash?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
hpaskal
Associate II
Posted on May 17, 2011 at 12:01

Hi !

I am using upsd3334d device with KEIL uVision2.

My bootloader project configs:

fs0: 0x0000 - 0x3FFF

fs1: 0x8000 - 0xFFFF page 1

fs2: 0x8000 - 0xFFFF page 2

...

fs7: 0x8000 - 0xFFFF page 7

rs0: 0x4000 - 0x5FFF

csiop: 0x6000 - 0x60FF

csboot0: 0x0000 - 0x1FFF

during the boot , the main flash is in Data space.

i wrote a boot code that runs on csboot0 and seems to wroke fine exept 2 problems:

1)I am using Flashcode.c file from the ST boot examples.

befor I program the main flash , I erased it with the erase function :

flash_erase_sector(0x0000);

for(page=1;page<=NumHexFiles;page++)

{

page_set(page);

flash_erase_sector(0x8000);

}

.

If this code is running after I burn the boot project with jtag , it is ok.

BUT if i try to run it not after a jtag burn, i stuck in the flash_erase_sector()

function.

what could be the problem ?

2)problem NO.2:

when i finish to wrote the main flash , I set the VM reg and need to jump to address 0.

if I stop and set the PC manually to 0 , i can see that it is OK and the new code is running ok.

but when the program trys to jump to loacation 0 , it dont work.

here is the jump routine :

void

SwitchMainFlash()

{

PSD8xx_reg.VM = 0x8C;

PSD8xx_reg.PAGE=0;

#pragma asm

ljmp 0x0000;

#pragma endasm

}

What can be the problem ?

Thanks

[ This message was edited by: hpaskal on 20-06-2004 18:33 ]
hanan54
Associate II
Posted on May 17, 2011 at 12:01

hi haim

In problem 2 try

SwitchMainFlash()

{

PSD8xx_reg.VM = 0x0C;

#pragma asm

jmp 0x0000;

#pragma endasm

}

try jmp insate of ljmp

In my project, I do the same and It''s work fine.

Did you put SwitchMainFlash in fixed address. if not put the line

?PR?SwitchMainFlash?ModulName(fixed address)

in BL51 locate in the line code.

the SwitchMainFlash procedure must be the only procedure in ModulName .

hanan

[ This message was edited by: hanan54 on 21-06-2004 08:44 ]
hpaskal
Associate II
Posted on May 17, 2011 at 12:01

Thank u very much hanan54 and HansDK!

it works .

this make sence cause u cant switch to main flash and expect to fetch another command from the second flash ...!

I still have the erase problem

can anyone help ?

[ This message was edited by: hpaskal on 21-06-2004 12:59 ]