2026-04-20 3:55 AM - last edited on 2026-04-20 4:13 AM by Andrew Neil
Are the pin configurations for TSV321RAILT and TSV321RILT exactly the same?
I'm having trouble finding this information in the datasheet.
Solved! Go to Solution.
2026-04-20 4:12 AM
Welcome @n_minakata, to the community!
The two order designations differ exclusively in the offset voltage, which is indicated by the inserted letter 'A'. The offset values are given in the data sheet, table 3 for VCC=3V and table 4 for VCC=5V.
The pin assignment is exactly identical for both.
Does it answer your question?
Regards
/Peter
2026-04-20 4:12 AM
Welcome @n_minakata, to the community!
The two order designations differ exclusively in the offset voltage, which is indicated by the inserted letter 'A'. The offset values are given in the data sheet, table 3 for VCC=3V and table 4 for VCC=5V.
The pin assignment is exactly identical for both.
Does it answer your question?
Regards
/Peter
2026-04-20 6:02 PM
I understand perfectly.
Thank you for your prompt reply.