cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-53L1A2 board doesn't work with VL53L1_GUI. Center is no problem, but other sides (not only LEFT but also RIGHT) didn't work. I purchased two connectors (2x5 box) and soldered them on the board. I connected breakout boards to LEFT and RIGHT.

TYomo
Associate II

If I selected CENTER, the measurement started well. But if I selected LEFT or RIGHT, the measurement seemed to be stopped even though start button was pushed.

Is it bug?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

Heck yes, it's a bug. We are working to get it fixed. Thanks for pointing it out.

(I'm guessing few people actually use the satellites or if the do, they don't complain much.)

We will get it fixed asap.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.