cancel
Showing results for 
Search instead for 
Did you mean: 

What's the minimum target size for VL53L1X and VL53L3CX ?

PQiu.1
Associate

Hi, i want to use VL53L1X and VL53L3CX  to detect a small size target (e.g finger,rope) at 1 meter away. i am wandering what's the minimum target size for VL53L1X and VL53L3CX ?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Julien NGUYEN
ST Employee

Hi

A finger at 1 m will be difficult to detect, actually the surface is too small and the distance is too long to have enough photons coming back even if the human skill has a quite good IR refelectance ~60%. Anyway, you have better chance with the L1X and the L3CX because the L1X has lens so better sensitivity. Just try it.

Thanks,

Julien


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.