cancel
Showing results for 
Search instead for 
Did you mean: 

What is the I2C bus capacitance of LIS2MDL and LSM6DSL?

JTomp.1
Associate II

I have both these devices on the same I2C bus and am trying to calculate the maximum pullup resistance.

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TBomb.1
Senior II

Hi, usually they are driven or left at high impedance, so the capacitance is mostly determined by the parasitic of the pcb on the I2C lines.

Pay attention to the max I2C speed. I believe you can go up to 100kOhm pullup, if you want to minimize the consumption.

\Tom

View solution in original post

2 REPLIES 2
TBomb.1
Senior II

Hi, usually they are driven or left at high impedance, so the capacitance is mostly determined by the parasitic of the pcb on the I2C lines.

Pay attention to the max I2C speed. I believe you can go up to 100kOhm pullup, if you want to minimize the consumption.

\Tom

ASbor.1
Associate

Hello All!

Is it possible to interrogate 30 sensors through the I2C expander without using an interrupt

 - LIS2MDL ? I can attach the diagram in the next message if necessary.