cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L0X

MSAMB.1
Associate III

What is the difference between signle and continuous mode ? someone can telle me please the real difference I'm using the VL53L0X

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

You probably mean the single and continouos ranging, right?

The datasheet provides quite detailed information:

Single ranging

Ranging is performed only once after the API function is called.

System returns to SW standby automatically.

Continuous ranging

Ranging is performed in a continuous way after the API function is called. As soon as the measurement is finished, another one is started without delay.

User has to stop the ranging to return to SW standby. The last measurement is completed before stopping.

Does it answer your question?

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.