cancel
Showing results for 
Search instead for 
Did you mean: 

STWINKT 1B bug in fft analys demo.

karakasali
Associate

In ultrasoun library has a bug. If change you in fft_app.h FFT_OUTPUT program is not compiled. Please change code like this

 

 

static void FFT_Thread(void const *argument)
{
  (void) argument;

#if (configUSE_APPLICATION_TASK_TAG == 1 && defined(TASK_FFT_DEBUG_PIN))
  vTaskSetApplicationTaskTag(NULL, (TaskHookFunction_t)TASK_FFT_DEBUG_PIN);
#endif

#ifdef DATA_TEST
  static uint16_t usbTestData = 0;
#endif

#if (FFT_OUTPUT == FFT_AVERAGE)
  uint16_t nAccTotal = 10;
  uint16_t nAcc = 0;
#endif

  FFT_Lib_Init(512, 0.5f);

  for (;;)
  {
    osSemaphoreWait(fft_data_input_sem_id, osWaitForever);
    FFT_Process(&audio_fft_instance, audio_fft_out);

#if (FFT_OUTPUT == FFT_RAW)
    if (com_status == HS_DATALOG_USB_STARTED)
    {
      USBD_WCID_STREAMING_FillTxDataBuffer(&USBD_Device, 0, (uint8_t *) audio_fft_out,
                                           sizeof(float) * audio_fft_instance.init_params.FFT_len / 2);
    }
#elif (FFT_OUTPUT == FFT_AVERAGE)
    arm_add_f32(audio_fft_out, FFT_Average, FFT_Average, audio_fft_instance.init_params.FFT_len / 2);
    nAcc++;

    if (nAcc == nAccTotal)
    {
      arm_scale_f32(FFT_Average, 1.0f / (float)nAcc, FFT_Average, audio_fft_instance.init_params.FFT_len / 2);
      if (com_status == HS_DATALOG_USB_STARTED)
      {
        USBD_WCID_STREAMING_FillTxDataBuffer(&USBD_Device, 0, (uint8_t *)FFT_Average,
                                             sizeof(float) * audio_fft_instance.init_params.FFT_len / 2);
      }
      memset((uint8_t *)FFT_Average, 0, audio_fft_instance.init_params.FFT_len / 2);
      nAcc = 0;
    }
#elif (FFT_OUTPUT == FFT_WEIGHTED_AVERAGE)
    uint32_t i;
    for (i = 0; i < audio_fft_instance.init_params.FFT_len / 2; i++)
    {
      audio_fft_out[i] = FFT_Average[i] * 0.97f + audio_fft_out[i] * 0.03f;
      FFT_Average[i] = audio_fft_out[i];
    }
    if (com_status == HS_DATALOG_USB_STARTED)
    {
      USBD_WCID_STREAMING_FillTxDataBuffer(&USBD_Device, 0, (uint8_t *)FFT_Average,
                                           sizeof(float) * audio_fft_instance.init_params.FFT_len / 2);
    }
#endif

#ifdef DATA_TEST
    uint16_t i = 0;

    int16_t *p16 = (int16_t *)dataOut;
    for (i = 0; i < 4; i++)
    {
      *p16++ = usbTestData++;
    }
#endif
  }
}

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
niccolò
ST Employee

Hi @karakasali ,

Welcome to ST community =)

thank you for your input, but would you mind explaining what is the problem with the default library?

Niccolò