cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IME002V2(HM301D) evaluation board settings for PC application(EDEN)

devnandan
Associate
Posted on October 26, 2016 at 17:33

I'm using a  STEVAL-IME002V2(HM301D) single lead ECG evaluation board. I do not use the ECG DB 15 connector, instead i make use of the RL,LA and RA leads in the board to connect the electrodes. I'm trying to get the heartbeats, as ECG signal waveform is not fully required for my project. currently i'm using only 3 electrodes(RL,LA,RA). Please help me with the settings through  which i can  get the heartbeats in the PC application (Eden application), which is provided with he evaluation board.I need to know the deafult settings of the board from which i can get heartbeats in eden application

#steval-ime002v2
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0