cancel
Showing results for 
Search instead for 
Did you mean: 

MKI119V1 building iNemo application

erik239955_stm1
Associate
Posted on February 01, 2013 at 08:32

I have a MKI-119V1 evaluation board and want to use the iNemo example application for IAR Embedded Workbench provided in

..\iNEMO Suite\Firmware\iNEMO_Project\iNEMO_Project\iNEMO_EWARM

But after compiling and downloading with DfuSe Demonstration nothing happens and the usb connection is lost. If I have understood it correctly I should at least see a Led blinking by uncommenting the following line in main.c:

//#define TEST_ENABLE

Can anyone give me an explanation how this works: 

Is the the Dfu always located at address 0x8000000 and the application at 0x8003000?

If I download a new application will it automatically be located at 0x8003000? Will the Dfu still be located at 0x8000000? Do I have to change anything in DfuSe?

Do I have to build both the Dfu and the application and combine these to get it working?

If anyone can give me a detailed explanation of how to get started with building and downloading i would be very thankful, but any help is appriciated.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0