cancel
Showing results for 
Search instead for 
Did you mean: 

LISD2E12 INT1_THS not changing tilt threshold

Joseph Lehman
Associate II
Posted on February 23, 2018 at 21:28

The INT1_THS register value does not seem to change the threshold at which an event is triggered. I can read and write the INT1_THS(0x32) so I know my writes are working. I poll the INT1_SRC register and watch the bits change so the position enable ints are working it is just that the threshold seems fixed not adjustable.

INT1_CFG = 0xCF to enable X & Y position triggering

INT1_THS = 0x20 = 0.5g or 30 degrees. (actual int flags trip around 0.94g/66 degrees)

Thanks in advance for any help.

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Joseph Lehman
Associate II
Posted on April 13, 2018 at 13:49

Solved! For those who follow this thread in the future.  In order to get a position threshold below 45 degrees or 0.7g to work, one of the axis must be disabled in the REG1_CFG so disabling in INT1_CFG is not enough, but the whole axis must be disabled in REG1_CFG