cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3MDL noise and maximum accuracy

arslanoglu
Associate II

In my system that found the heading angle using the LIS3MDL sensor, the maximum error value was 3 degrees using the ellipsoid calibration method. Also, although I used the sensor in low noise mode, I saw that the data in Matlab graphics was very wavy and noisy.
What is the accuracy value of the LIS3MDL sensor? What should I expect the max and average values to be? And what can I do to reduce noise?
Thanks for your help

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Federica Bossi
ST Employee

Hi @arslanoglu ,

What do you mean as very noisy? On which axis? From our datasheet the RMS noise should be 3.2 mGauss for X and Y axis and 4.1 mGauss for Z axis.

The accuracy depends on which is your FS, you can find it in the datasheet too.

If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.