cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DH12 Double Click Interrupt

Chithambaram Veerappan
Associate II
Posted on January 04, 2017 at 18:13

Hi All

I am having some difficulties in configuring the Double Click Interrupt on the LIS2DH12.

After power up, I am doing the following:

TEMP_CFG_REG = 0xC0

CTRL_REG4 = 0x80

CTRL_REG1 = 0x77

The above seems to work and provides sensible values for xyz axis when the PCB is at various angles. This suggests that the I2C bus is functioning correctly. 

Next I would like to enable click detection in the y- axis (any axis would do to start to prove the function works). I would like an interrupt on INT1 when a double click has occurred. INT1 is pulled up to 3.3 V via a 100 kOhm resistor.

I am doing the following in order to configure the Double Click feature

CTRL_REG3 = 0x80

CLICK_CFG = 0x08

CLICK_THS = 0x88

TIME_LIMIT = 0xFF

 //Not really sure the purpose of this, the datasheet is not really clear

TIME_LATENCY = 0xFF

 //Not really sure the purpose of this, the datasheet is not really clear

TIME_WINDOW = 0xFF  //Not really sure the purpose of this, the datasheet is not really clear

All other registers are left at their default values. 

I am then reading the CLICK_SRC register in a loop. I am checking to see if bit 6 is a 1, which indicates that an interrupt has occurred.

Looking at the INT1 pin on the scope, it appears to be toggling. I understand that the INT1 will switch after CKICK_SRC is read, however the value read back indicates that no double (or single) click interrupt has occurred. Looking at the datasheet I also thought that all the other interrupts were disabled by default. 

If anyone has any suggestions or thoughts or even a working basic configuration, it would be much appreciated.

Thank you

Kind regards

Chithambaram 

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on January 10, 2017 at 17:58

Hi Chithambaram,

I checked your configuration and I used the same on my board with connected LIS2DH12.

I works well. I see the interrupt is triggered on INT2 pin by logic analyzer if I hit or turn the sensor.

If this configuration is not working I suppose there is some hardware issue on your board.