cancel
Showing results for 
Search instead for 
Did you mean: 

I want check if Datecode 711D4 is year 2017 12 week. Please help check and reply me Thanks very much.

EYao.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @EYao.1​ ,

I can reply here since it might be of interest for other users.

Which product are you using?

Please note that, in general, the Datecode can be decoded as follows: 711D4

  • "7" means 2017
  • "11" means wk 11 2017
  • "D4" is the product code

So basically your product has been assembled (and the marking printed) in wk11, but the lot name is given by the test week, that could be wk12 in your case, so your guess should be effective.

-Eleon