cancel
Showing results for 
Search instead for 
Did you mean: 

Hi guys, Now I have some troubles with 2 VL53L1X that measure the distance at the same time but I can't init these sensor ?

PTam.2
Associate

Hi guys,

Now I have some troubles with 2 VL53L1X that measure the distance at the same time but I can't init these sensor ? Here my code I code on Esp32. I'm using SparkFun library

https://github.com/sparkfun/SparkFun_VL53L1X_Arduino_Library.git

#include <Arduino.h>

#include <WiFi.h>

#include <Wire.h>

#include <Ethernet.h>

#include <SPI.h>

#include <VL53L1X.h>

#define SHUTDOWN_PIN 2

#define INTERRUPT_PIN 3

#define Sensor1_newAddress 47

#define Sensor2_newAddress 45

SFEVL53L1X Sensor1;

SFEVL53L1X Sensor2;

uint16_t distance0, distance1;

// #define SHUTDOWN_PIN 2 // có thể mở

// #define INTERRUPT_PIN 3

#define XSHUT_pin1 33

#define XSHUT_pin2 32

void setup (void)

{

  Wire.begin();

  Wire.setClock(400000); // use 400 kHz I2C

  Serial.begin(115200);

  Serial.println("Begin.....");

    

  Wire.begin();

  Wire.setClock(300000); 

  pinMode(XSHUT_pin1, OUTPUT);

  pinMode(XSHUT_pin2, OUTPUT);    

   

  pinMode(XSHUT_pin1, INPUT);

  if (!Sensor1.init())

  {

    Serial.println("VL53L1X custom sensor, Failed to detect and initialize sensor1!");

    while (1);

  }

  delay(10);

  Sensor1.setI2CAddress(Sensor1_newAddress);

   

  pinMode(XSHUT_pin2, INPUT);

  if (!Sensor2.init())

  {

    Serial.println("VL53L1X custom sensor, Failed to detect and initialize sensor2!");

    while (1);

  }

  delay(10);

  Sensor2.setI2CAddress(Sensor2_newAddress);

   

    

  // Sensor1.setTimeout(500); // có thể mở

  // Sensor2.setTimeout(500);

  Sensor1.setDistanceModeLong();

  Sensor1.setTimingBudgetInMs(50000);

   

  Sensor2.setDistanceModeLong();

  Sensor2.setTimingBudgetInMs(50000);

}

void loop(void)

{  

  distance0 = Sensor1.getDistance(); // return distance 

  Sensor1.stopRanging(); //Stops taking measurements // after measure the first distance stop measurement

  Sensor1.clearInterrupt(); // Clear the interrupt flag // clear the interrupt 

   

  distance1 = Sensor2.getDistance(); // return distance 

  Sensor2.stopRanging(); //Stops taking measurements // after measure the first distance stop measurement

  Sensor2.clearInterrupt(); // Clear the interrupt flag // clear the interrupt 

   

  Serial.print("Distance 0: ");

  Serial.println(distance0);

  Serial.print("Distance 1: ");

  Serial.println(distance1);

     

  return;

}

Thanks for help

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

I didn't read all the code, but I have 2 suggestions.

1 - your MCU is much faster than the sensors, I think you will find a 'wait_for_booted' in that library somewhere.

You were turning the sensor on in one clock cycle and initializing it in the next. It's a good sensor, but it does have to boot up.

(or you can just wait a few milliseconds.)

2 - The other trick is that the I2C is generally specified by the write address - and those have zero's in the LSbit.

It's also a superstition of mine that I put more distance between the addresses. You are right that they have to be 2 apart, but I've had better luck with 10 appart.

Download

STSW-IMG017

2D LIDAR using multiple VL53L1X Time-of-Flight long distance ranging sensors.

It has an example of how we did 9 sensors. It will give you some ideas.

  • john

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.