cancel
Showing results for 
Search instead for 
Did you mean: 

Does lsm6dsox provide some pin similar as NRST for hardware reset?

YYuan.1
Associate II

Besides the SW_Reset in CTRL_3 register, can we also do the hardware reset for lsm6dsox through some pins? Or the power gate is only option we can use?

The chip worked perfectly on our device, however, in some rare cases, the registers, including whoami register, is not accessible. So we want to check if hardware reset is possible for this chip. thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TBomb.1
Senior II

Hi @YYuan.1​ , I believe that the only way to "hard" reset the chip is the power cycle. The only other way is the soft reset. But did you investigate the reason for the memory reading issue that sometimes occur?

\Tom

View solution in original post

2 REPLIES 2
TBomb.1
Senior II

Hi @YYuan.1​ , I believe that the only way to "hard" reset the chip is the power cycle. The only other way is the soft reset. But did you investigate the reason for the memory reading issue that sometimes occur?

\Tom

Eleon BORLINI
ST Employee

Hi @YYuan.1​ ,

Tom is right.

-Eleon