2020-06-10 9:59 AM
Hi community:
There is this driver provided on ST webpage for LIS2DW12:
leading to:
https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lis2dw12_STdC
The driver provided here does polling, but I need an interrupt based driver.
Can someone provide an INTERRUPT BASED driver?
Thanks!
2020-06-11 1:58 AM
Hi @CPeng.1 , but you can take inspiration from, for example, this other driver lsm6ds3_read_data_interrupt.c. You have to route first the DRDY signal on INT1 pin:
/* Enable interrupt generation on DRDY INT1 pin */
lis2dw12_pin_int1_route_get(&dev_ctx, &int_1_reg);
int_1_reg.int1_drdy_xl = PROPERTY_ENABLE; // INT1_DRDY bit in CTRL4_INT1_PAD_CTRL (23h) register
lis2dw12_pin_int1_route_set(&dev_ctx, &int_1_reg);and then manage the dataout read triggering the application processor with that interrupt signal
static int32_t platform_read_int_pin(void)
{
return HAL_GPIO_ReadPin(LIS2DW12_INT1_GPIO_PORT, LIS2DW12_INT1_PIN);
/* Please uncomment next line if interrupt configured on INT2 pin */
//return HAL_GPIO_ReadPin(LSM6DS3_INT2_GPIO_PORT, LSM6DS3_INT2_PIN);
}Regards