cancel
Showing results for 
Search instead for 
Did you mean: 

AIS2DW12 power consumption when SPI SDO left low after communications

JasonRrrr
Associate II

When I read the FIFO with SPI the SDO pin is sometimes left LOW. This causes a current leak through the internal pull-up. See pic attached showing 1 minute of readings every 800ms. As you can see the current is high every time the SDO pin is low. I assume the internal pull-up is causing the current.

I've read the data sheet and the application note AN5326 but I cannot see why this happens.

I'm using ODR 25HZ with Power mode 4, +2G range and continuous FIFO. SPI 4-wire. NRF52840. I have tested the NRF52840 current draw and determined that the accelerometer is drawing the current.

To hack it lower before sleeping, I've set -1 (oxFF) to my Z_OFS_REG and I read from the Y_OFS_REG (this register precedes Z_OFS_REG). This results in the trailing SDO bit always being high at the end of the SPI read. This leaves the SDO line HIGH which avoids the problem. I would like to know if there's a more conventional way of fixing this.

I've tried all 4 SPI modes and I've tried SPI frequencies 125khz, 4Mhz and 8Mhz.

My accelerometer is the STEVAL-MKI206V1 breadboarded with an nrf52840 dongle. 4 wires from accelerometer to dongle. no additional components.

Any help is greatly appreciated.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Ok, let's wait for the LIS3DH samples, hope they will arrive soon.

-Eleon