Skip to main content
Matt Bennett
Associate
February 8, 2019
Question

Why does ST's LoRa driver continue to break EU TX power regulations?

I opened a support ticket with ST back in October (2018) highlighting a bug in their driver code that adds +1 dBm to a user's TX power request. If a 14 dBm TX power (EU limit in most 868 LoRa bands) is set by the user through the I-CUBE-LRWAN driver API, the driver code actually sets the SemTech RF IC's register setting for 15 dBm, which (unknown to the user) would break EU TX regulations. I received no response until December (2018) where it was simply said my bug fix had been passed-on.

This topic has been closed for replies.

1 reply

Matt Bennett
Associate
February 8, 2019

[Continued, form submits when you press enter?] I noted the new release of the I-CUBE-LRWAN (1.2.1) still did not include this fix. I opened a new support ticket again highlighting the issue (and including the file name, line number and simple code fix). Unfortunately this time, whoever is at the other end of the ST support for this case is INSISTING they will do nothing unless I provide an "image of the RF signal as displayed on a calibrated Spectrum Analyzer". I have explained multiple times their driver is asking the SemTech RF IC (SX1276) a TX power level in dBm directly to its register, that is wrong. It is very fair for me to assume the SemTech chip will perform as it is certified to do and output the TX power it has been asked to (which it still within its own specification). The clear issue is ST's driver is passing a HIGHER TX power level than set by the user through their API. It should NOT require an (expensive) calibrated RF analysis to request that ST Microelectronics fix a bug in their code, that is at the very least ASKING the SemTech RF IC to transmit at levels that are above EU limits against the wishes of the programmer. What a very stubbon and anti-customer line for ST Support to be taking. For reference, my support case IDs were 00067813 (where I provide full code details, datasheet references and explanations) and 00072508 (current, "we don't care unless you prove the RF output is illegal", case).