Skip to main content
Visitor II
September 4, 2023
Question

What are the units of the characteristic data timestamps?

  • September 4, 2023
  • 0 replies
  • 860 views

According to the characteristic/features section in this BlueSTSDK documentation page, characteristic data has a 2-byte timestamp. What are the units of this timestamp? In other words, what does each tick in the timestamp represent?

The timestamp goes from 0 to 2^16 - 1, then resets. In the data I have collected, the timestamp appears to reset every 2 seconds. This would imply one tick is 2 s / 2^16 ≈ 3.052e-5 s. However, I want to verify exactly what the reset period is. For maybe, e.g., the data is actually resetting every 2.048 s = 2^11 ms, implying one tick is 2^11 ms / 2^16 = 3.125e-5 s.

This topic has been closed for replies.