cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IDB007V1M, SPBTLE-1S Not working

MikeP
Senior

Hi,

I have bought a STEVAL-IDB007V1M so i can learn how to incorporate BLE into my project but im having problems.

The board isn't being picked up on BlueNRG-1 Navigator but it is being picked up on BlueNRG-2 Navigator. - Im not sure if this is a problem?

BlueNRG-2 Navigator allows me to flash and run, so i loaded on the beacon to see if i can find the board on my iPhone, it successfully flashes but i cant see anything on any BLE App.(BLE Scanner, LightBlue)

I have read the other posts that say that the HS_SPEED_XTAL_32MHZ should be 32MHz, but looking at the project code it looks like it is set to that.

  

Any help would be appreciated.

Kind Regards,

Mike

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PDeck.2281
Associate III

Anyone know the answer to this?

@Thiago REIS​