2025-11-14 6:57 PM
您好!目前我有几个STM8500+STLD1直流载波通信的疑问,请麻烦回复!
1:我通过STLD1发送差分信号,通过高压电容耦合在DC48V和DC48V_GND上,再在接收端进行接收,应该没啥问题吧,理论传输距离可以达到3km吧,有没有完整一些的参考原理图设计,因为官网提供的手册原理图不完整
2:stm32f401通过uart与st8500进行通信,调用at指令或者api接口就能使用st8500吗,还是我需要在st8500上面进行编程或者要下载固件才能使用