cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF01SA IBSS

pietro
Associate
Posted on February 25, 2015 at 12:08

Hi, I'm using STEVAL-IDW001V1 and STEVAL-PCC018V1 boards.

I set up wifi into IBSS mode named ''ADHOC'' but I cannot detect it from the telephone or browser.

I've the impression I'm not creating the ADHOC network. Where's the issue?

I'm attaching data. 

+WIND:2:Reset

+WIND:1:Poweron (141106-0950875-SPWF01S)

+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc.  All rights Reserved.

+WIND:3:Watchdog Running

+WIND:0:Console active

+WIND:32:WiFi Hardware Started

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete (0x0)

+WIND:19:WiFi Join:16:BD:EC:00:B3:C5

+WIND:25:WiFi Association with 'ADHOC' successful

+WIND:51:WiFi Handshake Complete

+WIND:24:WiFi Up:192.168.1.101

# Status & Statistics:

#  version = 141106-0950875-SPWF01S 

#  reset_reason = 2

#  conf_flag = 5

#  system_uptime = 103

#  system_sleeptime = 0

#  gpio_enable = 0

#  captiveportal = 0

#  wifi_state = 10

#  wifi_bssid = 16:BD:EC:00:B3:C5

#  wifi_aid = 0

#  wifi_channelnum = 6

#  wifi_sup_rate_mask = 0x003FFFCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_chan_activity2 = 0x00000020

#  wifi_max_tx_power = 18

#  wifi_reg_country = 

#  wifi_dtim_period = 0

#  wifi_sleeping = 1

#  wifi_num_assoc = 0

#  ip_ipaddr = 192.168.1.101

#  ip_netmask = 255.255.255.0

#  ip_gw = 192.168.1.1

#  ip_dns = 208.67.222.222

#  ip_sock_open = 0

#  ip_sockd_port = 0

#  free_heap = 21656

#  min_heap = 20312

#  current_time = 2342

OK

# Dumping All Configuration Keys:

#  nv_manuf = ST

#  nv_model = SPWF01SA1

#  nv_serial = 4313D25167

#  nv_wifi_macaddr = 00:80:E1:FF:BA:C7

#  blink_led = 0

#  wind_off_low = 0x00000000

#  wind_off_medium = 0x00000000

#  wind_off_high = 0x00000000

#  user_desc = anonymous

#  escape_seq = at+s.

#  localecho1 = 0

#  console1_speed = 115200

#  console1_hwfc = 0

#  console1_enabled = 1

#  sleep_enabled = 0

#  standby_enabled = 0

#  standby_time = 10

#  wifi_tx_msdu_lifetime = 0

#  wifi_rx_msdu_lifetime = 0

#  wifi_operational_mode = 0x00000011

#  wifi_beacon_wakeup = 1

#  wifi_beacon_interval = 100

#  wifi_listen_interval = 0

#  wifi_rts_threshold = 3000

#  wifi_ssid = 41:44:48:4F:43:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_ssid_len = 5

#  wifi_channelnum = 6

#  wifi_opr_rate_mask = 0x00003FCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_mode = 2

#  wifi_auth_type = 0

#  wifi_atim_window = 0

#  wifi_powersave = 0

#  wifi_tx_power = 18

#  wifi_rssi_thresh = 0

#  wifi_rssi_hyst = 0

#  wifi_ap_idle_timeout = 120

#  wifi_beacon_loss_thresh = 10

#  wifi_priv_mode = 0

#  wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_key_lens = 00:00:00:00

#  wifi_wep_default_key = 0

#  wifi_wpa_psk_raw = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wpa_psk_text = 

#  ip_use_dhcp = 0

#  ip_use_httpd = 1

#  ip_mtu = 1500

#  ip_hostname = iwm-FF-BA-C7

#  ip_apdomainname = captiveportal.net

#  ip_ipaddr = 192.168.1.101

#  ip_netmask = 255.255.255.0

#  ip_gw = 192.168.1.1

#  ip_dns = 192.168.1.1

#  ip_http_get_recv_timeout = 3000

#  ip_dhcp_timeout = 20

#  ip_sockd_timeout = 250

OK
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
danielkorbes
Associate II
Posted on February 25, 2015 at 17:56

Pietro, I had the same problem.

To solve it I need to update the module. Try v3.3.

And update it OTA. Using UART I ''brick'' the module...

Gerardo GALLUCCI
ST Employee
Posted on February 26, 2015 at 08:48

IBSS was included into FW 20140805, namely FW3.2

Gerardo GALLUCCI
ST Employee
Posted on February 26, 2015 at 10:08

Did you set a static IP address also on smartphone?

Depending on OS, this step is mandatory.

This step is not needed, for example, using iOS.
pietro
Associate
Posted on February 26, 2015 at 11:27

Ok, thanks, understood. It works.

Thank you Gerardo!

Bye