2017-10-05 3:38 AM
Hi,
sometime I get the error 'Failed to resolve name'. I always call the same address - so the address is valid. If I get this error I have to reset the module.
What failures cause this error?
BR,
Flow
Solved! Go to Solution.
2017-11-10 10:50 AM
Internal buffer for DNS reply was a little bit too small into FW3.5 (compared with FW3.4)
It has been increased into FW3.5.3. This is why it's working again.
2017-11-09 10:36 PM
If anybody else will have this problem:
I still do not know, why this error occurs. But it seems to be a bug in FW 3.5. After updating some modules to FW 3.5.3 I didn't get this error again...
2017-11-10 10:50 AM
Internal buffer for DNS reply was a little bit too small into FW3.5 (compared with FW3.4)
It has been increased into FW3.5.3. This is why it's working again.
2017-11-13 11:14 AM
Thanks for explanation.
Are further updates for the SPWF01 module planned?
2017-11-14 3:07 AM
Yes, sure. Q1 2018.
2017-11-14 3:21 AM
Great! Early or late Q1 2018?
If it is early, I will wait and do not bring out the FW 3.5.3...
2017-11-14 6:39 AM
No date at the moment.
It's suggested to update, but it's not mandatory. It's up to you...
2018-02-02 2:17 AM
Hi Gerry,
we have Q1 2018: Can you tell me when the firmware update will be released?
Thank you.
BR,
Flow
2018-11-05 7:28 AM
Sorry for the delay, I missed the post.
FW rel 3.6.0 is available on st.com
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.