2016-10-04 7:58 AM
Hi,
I use the SPSGRF module in 868MHz Narrowband. I search to send packet with this configurations : - Fc = 869.2375MHz- Fdev = 2.7 kHz- Datarate = 4.8 kBit/s- Number of channels : 0- Spacing channel : don't care ? - Modulation : GFSK_BT05So for my receiver a set : - Channel filters : 11,0 kHz > (2*Fdev + datarate) ~ 10,4KHz- SQI / PQI : Disable - RSSI Threshold : -20 dBm.In this configuration I receive nothing. In my Spectrum analyzer, I see a signal when I transmit something, but receiver doesn't see : Preamble, Sync Word ... So which parameter I miss to configure for make a reception ? Something hide ? Or it's my transmit who is no good ? I think is not channel filter the problem... Regards,Lo�c #spirit1-rx-tx-receive-transmit