cancel
Showing results for 
Search instead for 
Did you mean: 

SP1ML packet

sfantuzzi
Associate
Posted on April 05, 2016 at 18:13

I need to send complete (and receive) custom packet through the module SP1ML to cummunicate with another SPIRIT1 board (protocol is fixed). This protocol is based on ''Basic Packet'' (no StAck nor Wmbus) with :

12 bytes preamble

2 bytes Sync Word

variable length payload

No address sent

No Control sent

CRC 0x8005

Is it possible to obtain this with the SP1ML module?

We used the STEVAL board to communicate without problems.

Is it possible to do this with SP1ML with original Fw ?

Thank you very much

Best Regards

Simone

#spirit1-sp1ml-dongle #spirit1-sp1ml
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0