cancel
Showing results for 
Search instead for 
Did you mean: 

S2-LP: Minimal deviation for GFSK

TheMaksimys
Associate

Hi everyone!

We are trying to launch the GFSK reception on S2-LP in the basic mode. We have noticed that by reducing the deviation to 10 kHz most of the received packets gets discarded and even those accepted have at least 2-3 bits of errors. This behavior intensifies as we reduce the deviation even further. Due to the specifics of project FEC, CRC and other channel coding algorithms are not considered. The goal is to understand up to which deviation the reliable reception is possible. S2-LP is tested in pair with certified SDR GFSK transmitter, frequencies are synchronized, RSSI is within the allowed range with good margin.

If there are specific register settings that could help to improve the reception quality or you are having similar issues, please let us know by replying to this post.

0 REPLIES 0