cancel
Showing results for 
Search instead for 
Did you mean: 

KEIL Linker error while compiling en.stsw-bluemic-1 example code

Skada.3
Associate III

Hi

I am using example code for Bluenrg-1 is BlueNRG1_PER_BlueVoice

While compiling I am getting linker error in Keil IDE V5.25.2.0

errors are as below.

.\BlueVoice-BlueNRG1\BlueVoice-BlueNRg-1.axf: Error: #5: cannot open source input file "C:\Users\Ayu": No such file or directory

C:\Users\Ayu: 0 warnings, 1 error

.\BlueVoice-BlueNRG1\BlueVoice-BlueNRg-1.axf: Error: L6636E: Pre-processor step failed for '.\BlueNRG1.sct'

.\BlueVoice-BlueNRG1\BlueVoice-BlueNRg-1.axf: Error: L6372E: Image needs at least one load region.

How to resolve this error.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Does that directory exist? Does your User directory have any not ASCII characters or spaces in it?

Create a C:\Keil\BlueVoice directory, and unpack the software there are and try building it.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Skada.3
Associate III

getting solved by moving project folder in C driver.