cancel
Showing results for 
Search instead for 
Did you mean: 

HTTP POST on a secure connection

Matteo Pezzoli
Associate II
Posted on April 27, 2017 at 09:52

Hi,

I'm currently using the SPWF01SA module to make a POST request on a server. My tests using

http://httpbin.org/

went smoothly, but as soon as i try to make the request on the actual server, it responds with an error 307 (temporary redirect). My fear is that the server is forcing me to make a secure connection (as in forcing me to make the request on ' instead of ').

I tried using the entire uri ('

') as an argument of the AT+S.HTTPREQ command, but in that case the module is responding with 'host not found'.

So i guess my question is: is it possible to force the request to be on a secure connection? Or should i avoid the issue by manually opening a secure socket and then writing my request?

Thank you

Matteo

#http #spwf01s
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Gerardo GALLUCCI
ST Employee
Posted on April 27, 2017 at 11:30

Ciao Matteo,

HTTPS is not part of SPWF01S offer. You need to open a secure socket, and SOCKW/Q/R.

SPWF04S offers more...

Posted on April 27, 2017 at 11:55

Ciao Gerardo,

I would gladly use the SPWF04S, but we are unable to at the moment. I imagined the solution was to manually use the sockets, no problem there. I'm still encountering some difficulties, but i think those are server-related and not module related, so i will sort them out with the server owners. Thank you again for your time.

Matteo