2020-11-13 2:29 AM
Hi,
I work with the Nucleo-L476RG and the X-Nucleo-BNRG2A1 (BlueNRG2) and I would like to pair and bond this device to a Nordic nrf52840.
I followed the programming guideline and succeed to have a bond the devices. The BlueNRG2 is central and the Nordic is peripheral.
My problem is when I reconnect the devices, I have to start encryption with the "hci_le_start_encryption" function but I don't know how can I get the parameters needed for this function (i.e Random_Number, Encrypted_Diversifier, Long_Term_Key) which are used for the first pairing.
I tried to get the LTK with:
aci_hal_read_config_data(CONFIG_DATA_ER_OFFSET, <k_len, long_term_key);But I am not sure this is the good way.
And I have no idea how can I get the encryption diversifier.
Thank you for your help.