cancel
Showing results for 
Search instead for 
Did you mean: 

How can I change MTU value on my BLUENRG-M2 module

JPark.16
Associate

I want to change the MTU value.

As far as I checked through the manual, the mtu value is confirmed through aci_gatt_exchange_config().

I want to change the MTU value set at this time.

It seems that it can be set when the stack is initialized, but there is no BlueNRG_Stack_Initialization_t variable in the example code.

I tried changing the ATT_MTU value in bluenrg1_gatt_server.h but it didn't work.

Any help would be greatly appreciated.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Winfred LU
ST Employee

Take the DK 3.2.1 DTM project for example,

BlueNRG_Stack_Initialization() is called in DTM_StackInit(), located at DTM_boot.c line 591.

MTU can be modified in BlueNRG_Stack_Init_params, located at DTM_config.h line 160.

DKopp.2
Associate III

I have run into the same problem. I cannot find BlueNRG_Stack_Init_params. I'm using a X-NUCLEO-IDB05A2 evaluation kit with Nucleo-F303ZE STM evaluation board. Ive downloaded the software pack X-CUBE-BLE1 1.6.2.4. I dont have a config.h file where I have update parameters.

Any Help will be appreciated.

Winfred LU
ST Employee

BlueNRG-MS does not support data length extension.

Even though, i think it is possible to have a larger ATT MTU. The frames will be fragmented.

ATT_MTU is define in bluenrg_gatt_server.h

I didn't go deep into this. Not sure if modifying this is enough. But it would be a good start.