cancel
Showing results for 
Search instead for 
Did you mean: 

FOTA with IoT kit discovery node

DSabo
Associate III

I'm trying to get basic FOTA working with the example binary from en.fp-cld-azure download (Azure_IoTCentral_BL.bin).

I have the example binary loaded on the board and successfully connecting and communicating with my Azure IoT Central app.

I added the update command with the field name "FirmwareUpdate" and a text input field with the field name "FwPackageUri"

To do a basic test, I uploaded the binary to google drive and then sent the firmware update command with the URL to the binary, but it is failing (see errors below).

Not sure where to go from here as I thought this would be a simple start. I made sure that the google link is public so permissions shouldn't be an issue.

URL I used:

https://drive.google.com/file/d/1ird5B47Gq-e_SYX6hq5piiRBeszj_w6t/view?usp=sharing/Azure_IoTCentral_BL.bin

Log:

Received firmware update request. Use package at: [https://drive.google.com/file/d/1ird5B47Gq-e_SYX6hq5piiRBeszj_w6t/view?usp=sharing/Azure_IoTCentral_BL.bin]

Channel 1 for Timer 1 stopped

Download FOTA from: HostName=[drive.google.com] Type=[Secure] port=[443] File=[/file/d/1ird5B47Gq-e_SYX6hq5piiRBeszj_w6t/view?usp=sharing/Azure_IoTCentral_BL.bin]

Ok reported State [2]: Downloading

-->DeviceTwin CallBack [2]: Status_code = 204

Ok io_interface_description

Ok xio_create

onOpenCompleteFOTA

Ok xio_open

onSendCompleteFOTA

Ok xio_send HEAD Request

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

(Content-Length:) Full OTA size=0

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err... retriving the Full OTA Size...(Content-Length:)

Err During FOTA... Sorry retry...

Ok reported State [3]: DownloadFailed

-->DeviceTwin CallBack [3]: Status_code = 204

The Board will wait 5 Seconds before to send Sensor Data again

Channel 1 for Timer 1 started

Ok reported State [4]: Running

IoTHubClient_LL_SendEventAsync accepted message [27] for transmission to IoT Hub.

Confirmation received for message [27] with result = IOTHUB_CLIENT_CONFIRMATION_OK

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0