cancel
Showing results for 
Search instead for 
Did you mean: 

extending the range of bluenrg

blacklabstech
Associate
Posted on April 22, 2015 at 21:22

I am developing an application for bluenrg that requires extended range. Is there a way to configure the bluenrg such that it outputs on two of the test pins when the transmitter and receiver are turned on so that an external power amplifier can be hooked to the bluenrg? I notice that in the IFR area there is a byte called GPIO config but not information on what it does?

Does anyone else have any experience with extended range on the bluenrg?

#bluenrg-range
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on May 11, 2015 at 12:53

Hi tekky,

it's not possible to work with a FEM of BlueNRG.

regards,

GM